12/28/2017 4:01 PM | |
Joined: 3/15/2017 Last visit: 3/20/2024 Posts: 1 Rating:
|
Installing a S7-400H system. Using the 10km long distance sync modules, and need to know what kind of backbone fiber optic cable is required between PLC separated by 1km. The backbone will terminate in patch panel at each end, and patch cord used to connect to sync modules. What connector type required to the sync modules (LC?)? ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 12/31/2017 10:43:34 AMNew subject after splitting |
|
1/1/2018 5:06 PM | |
Joined: 5/28/2008 Last visit: 7/4/2024 Posts: 4510 Rating:
|
Hello, In the sync module side, you need LC end. Please check this link to see the all FO types: https://support.industry.siemens.com/cs/ww/en/view/35146578 And you will need to use patch panel with all accessories like couplers, connectors / Pig tails and also fiber optic cable. Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
Follow us on