1/1/2023 3:48 AM | |
Joined: 9/9/2015 Last visit: 6/24/2024 Posts: 727 Rating: (273) |
Hi Aswin Kumar, Yes, it is possible. Then it will be PLC + SCADA methodology. Extra works on SCADA such as 1. Diagnostic features of IO module 2. faceplate and block icons for all the valves, AI monitoring, pumps, DI 3. without auto generation of block icons, picture hierarchy 4. a lot of double engineering works involved between PLC and SCADA |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on