12/3/2008 7:15 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 11/17/2008 Last visit: 1/30/2024 Posts: 8 Rating:
|
Hi Dears How are you ? I want to select a redundant S7-414H for a PMS(Power Managament System) My I/O Counting is : 1256 :DI 448 :DO 163 :AI ET200M: 9 But I have just seen a catalog of siemens with strange information: this Link: https://www2.sea.siemens.com/Products/Process-Automation/Product/SIMATIC+PCS+7/Automation+System+Hardware+Controller/Automation+System+Hardware_Controller.htm contains:
Note The values listed here are not maximum AS-specific values for their respective model, they represent one typical distribution of the totally available for a representative mixture of I/O. Individual calculation of system capacity and performance is possible for actual systems using the configurator software present on the current CD-ROM of the interactive catalog CA 01. if really these are true , I cant use oneS7-417H too By the Way I Just want to know about Applicable Limitation of I/Os for S7-414 with Max Expanding Memory(of course for Timers,FBs,PIDs,..... and software Lisence I have to ConsiderMy Process) Thanks a lot |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
12/3/2008 10:55 AM | |
Joined: 9/1/2005 Last visit: 8/1/2024 Posts: 4104 Rating:
|
closed cause question posted twice. The second thread with the subject s7-400 typical system capacity?is published within the conference Process Control Systems SIMATIC PCS 7. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on