2/26/2019 10:41 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
I had a look in the FW-update-notes of your PLC: Download Betriebssystem Updates V4.5H CPU412-3H / CPU414-4H / CPU414-4H PG / CPU417-4H and you are right, you have to do it step by step when you want to do it in RUN. This is a special redundant 400H thing. See in the entry:
But when you want to update the PLC in Stop, you can just updat to the latest version. hope this helps, regards, |
Last edited by: mopS04 at: 2/26/2019 10:42:00 AMFCK WAR! |
|
This contribution was helpful to1 thankful Users |
2/18/2021 10:51 AM | |
Joined: 9/1/2017 Last visit: 12/20/2023 Posts: 156 Rating: (19) |
Hi Download Operating System Updates V4.5H CPU412-3H / CPU414-4H / CPU414-4H PG / CPU417-4HRegards Hosein |
Last edited by: Jen_Moderator at: 02/18/2021 11:31:14Optimized link. |
|
5/13/2021 7:23 PM | |
Joined: 11/29/2014 Last visit: 4/9/2024 Posts: 96 Rating: (23) |
Can you share it i also required same |
5/13/2021 7:37 PM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32954 Rating: (4073) |
On the link page is it. |
5/13/2021 8:09 PM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32954 Rating: (4073) |
Okay, I see it .. Then start a Support Request. |
Follow us on