5/11/2017 9:51 AM | |
Posts: 69 Rating: (0) |
Hi, I created a new data block in the TIA Portal. Declared the static variables test (integer, starting value 5) and test2 (integer, starting value 10). Using the S7-Node I can read those values without a problem. But if I change the starting values in the TIA Portal and Load it in my device, the S7-Node still reads the old values (I did deploy again). On top of that, if I add a random Variable to read in my S7-Node (e.g. integer asdf) which doesn't exist in TIA, the S7-Node still gives me an output for the variable which is similar to the var test. Where is the Problem there? Anyone experienced the same? BR ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/11/2017 10:35:29 AMNew subject after splitting |
|
Follow us on