6/30/2017 9:12 AM | |
Joined: 7/9/2015 Last visit: 4/17/2025 Posts: 4249 Rating:
|
Hi, which Version of PCT do you use? Only V3.4 or the newest V3.4 with Update 2. -> Please check the following entry for downloading the newest Version: S7-PCT V3.4 HF2 for IO-Link MasterRegards, Towome |
|
|
6/30/2017 9:21 AM | |
Posts: 4 Rating:
|
Hi, I use the newest V3.4 with Update 2. |
7/3/2017 9:46 AM | |
Posts: 4 Rating:
|
Hi, I run S7-PCT by right-clicking the Io-Link master, but I have the same problem. Thank you for the answers. |
Last edited by: TomasHanus at: 7/4/2017 6:36:05 AM |
|
7/10/2017 7:23 AM | |
Posts: 4 Rating:
|
I have a S7 PCT V3.4 with Update 2 installed. |
8/7/2017 2:17 PM | |
Posts: 7 Rating:
|
Excatly the same problem here.. Using newest software, S7-1215C with SM1278 module. Impossible to communicate with the SM1278 module ??? |
8/22/2017 8:22 PM | |
Posts: 9 Rating:
|
Hello! The same problem. TIA Portal 14 Sp1 Upd2, the same ET200SP IO-Link master. Interface module: CPU1510SP-1 PN 6ES7510-1DJ01-0AB0. Regards - Adrian |
Follow us on