1/19/2023 3:31 AM | |
Joined: 10/19/2022 Last visit: 9/10/2024 Posts: 5 Rating: (0) |
Hi, I had been using PLCSIM Advanced V4.0 with a trial license without a problem and decided to get a floating license. After installing the floating license I'm not able to power ON the PLC instances. Two error messages pop up:
What I've tried until now without success:
Windows version that I'm using: Windows 10 Professional 22H2. I know that 22H2 is not listed as a supported OS for V4.0 but since it was working with the trial license I thought there wouldn't be any problems. Has anyone ran into the same issue? Could anyone shed some light on this problem? My kids are crying because they can't run their simulations Thanks! |
1/19/2023 9:30 AM | |
Joined: 2/17/2020 Last visit: 9/12/2024 Posts: 1058 Rating: (192) |
Hi dcastillo93, Try to remove the Trial license by following this FAQ: |
A rating will be well appreciated. |
|
Follow us on