5/19/2011 11:43 AM | |
Posts: 30 Rating: (0) |
Hi,
I'm working on programming a PLC program in Step7. For wich I need to calculate an average value. First I have 144 samples in a DB8 and second I have 180 samples in a DB9. So I need a block wich can just say: ADD all the samples in DB8 and DEV them by the number of samples (= DB8.DBW12?). And the same for DB9. So I found a block that might do the trick at: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=39333121&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW I put the file in my program and I hit compile STL source file. When I do so I get 6 error's: E Ln 000026 Col 013: Syntax error at #RESET. E Ln 000027 Col 013: Syntax error at _001. E Ln 000034 Col 013: Syntax error at ;. E Ln 000043 Col 013: Syntax error at #BY_VALUE_CHANGE. E Ln 000044 Col 013: Syntax error at nmw. E Ln 000052 Col 013: Syntax error at ;. Now I don't know how to fix this and so I'm stuck at this point. I'm not a great programmer and I can only work with FBD and not with STL so if somebody would know a solution I would be very thankful. Thanks in advance. Kind regards, MatthiasV |
5/19/2011 12:15 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, For Step7 the right link is http://support.automation.siemens.com/WW/view/en/19345299 And another one - http://support.automation.siemens.com/WW/view/en/1021364 Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/19/2011 12:17 PM |
|
5/19/2011 1:15 PM | |
Posts: 30 Rating: (0) |
Thanks for the quick response UMENCHO. The second link you send me is the one I tried to use in the program but like I said I had 6 errors that I described in the above post. This one looks like the easiest way for me to program because It's for a project at school in wich I need to every step in the program. The first link looks a little hard for me. I can open the file but it doesn't allow a FBD view and only STL view. And like I said I reallydon't know anything about STL programming :s. Do you maybe know a way to make the second link work without the errors I'm having? Or is there a simple explanation for the first link that I could understand without any knowledge of accu, STL, ...? Kind regards, MatthiasV |
5/19/2011 1:25 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
My suggestion is to follow MM1234' answer. There everything is explained very well with details. Meanwhile if you have still troubles of course I could try to do compiling of source code on my PC and attch here the result. But really you can to do it alone. Just follow the MM1234. Best regards, Hristo Mihalev |
This contribution was helpful to4 thankful Users |
Follow us on