3/7/2019 3:50 PM | |
Joined: 9/27/2006 Last visit: 8/8/2024 Posts: 12273 Rating: (2680) |
Hello PedDa34; You will have to provide more information if you need our help. What communication protocols do your Delta PLCs support presently? A S7-1500 CPU (6ES7516-3AN01-0AB0, in your case) can support Profinet, Modbus/TCP, TCP/IP or UDP/IP directly on its integrated Profinet port. Profibus-DP on its integrated Profibus (RS-485) port; with an additional serial processor it will support Modbus RTU( over RS-232, RS-422 or RS-485). https://support.industry.siemens.com/cs/ww/en/pv/6ES7516-3AN01-0AB0/td?dl=en Do your Delta PLC match any of these supported protocols? Hope this helps, Daniel Chartier |
Follow us on