6/27/2010 5:23 PM | |
Joined: 5/28/2008 Last visit: 4/26/2025 Posts: 4520 Rating:
|
Hello, If the data to be shared between CPUs is less than or equal 22 byte, then the simplest way to share them is GD communication "Global Data Communication" Pleas see this FAQ: Basic communication between CPUs with global data And also this thread Hope this helps. |
Ayman Elotaify |
|
6/27/2010 6:43 PM | |
Joined: 1/17/2006 Last visit: 4/3/2025 Posts: 554 Rating:
|
Hello LittleJohn, In the following links you can find informations about networking CPU in Ethernet. Communication with SIMATIC S7 S7 Connections between CPU's with Built in Ethernet Port How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange on the S7-300? And below you can find a very good thread answered byour colleague and Platin Expert Wizard: /tf/WW/en/Posts/38483 Best regards. |
"Educate the children and it won't be necessary to punish the men." |
|
This contribution was helpful to
1 thankful Users |
6/29/2010 9:28 AM | |
Posts: 23 Rating:
|
Thanks |
Follow us on