Industry Online Support
Technical Forum
5/31/2012 8:05 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, The simplest way in my opinion is the following: - create a project where both CPUs are in that one project - open NETPRO (Step 7 classic) or the network view (TIA portal)andcreate an S7 connection between both systems. Be sure that the connection configuration data is loaded in both CPUs. - use in your program the functions for S7 connections (PUT, GET, BSEND/BRCV, ...). Be sure you use the S7-300 version of these blocks (instead of the CP versions of these blocks) Both have however the same parameters. An example interconnecting two 317-PN can be found here: http://support.automation.siemens.com/WW/view/en/22867279 There is no difference with a 315PN (just the CPU type in HWconfig). |
Best regards |
|
6/1/2012 1:20 PM | |
Joined: 3/16/2012 Last visit: 5/1/2024 Posts: 34 Rating: (0) |
thanks so much. |
Follow us on