2/11/2009 4:52 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Let's start with Which types of connection/protocols are supported as standard by S7-300/400 CPUs and the CPs? So existing DP/DP coupler is not useful in your case. In the other project with 3 Cp443-1 and 3 CP443-5 is more interesting. How is organized communication between them? profibus? Ethernet? Other way connect them via MPI, but it depends from quontity of data and distance between 2 of CPU. You can connect one of CPU from first project and one of CPU from second project. But in advance you must collect the data from each parther on each project. For me this way is not so good and useful, too many restrictions. Look at Options for communications via MPI Perfect way for me is to buy other 2 CP443-1 and connect all CPU in one network. Easier, but expensive. regards |
2/20/2009 11:06 AM | |
Posts: 88 Rating: (0) |
if I want to communicate via profibus, how ccan I do this. |
Follow us on