4/21/2012 10:38 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
Please see the attached and the below parts let me know, if the below parts are Ok for the attached system
AttachmentArchitecture.zip (580 Downloads) |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Last edited by: O_Moderator at: 4/24/2012 12:05 PMnew subject after splitting from /tf/WW/en/Posts/72780#top |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
4/23/2012 6:02 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
Hello Experts, I have attached the hardware configuration, per the above thread BOM, I have compiled and saved it. I do not have the actual hardware, so can't test it, could you please take a look at the attached and see if everything is all set or I have missed something. Your help in this regard will be highly appreciated, Attachmentsimatic h station(1).zip (551 Downloads) |
Last edited by: Lucky123 at: 4/23/2012 6:05 PMuploaded attached |
|
4/24/2012 12:39 PM | |
Joined: 12/1/2009 Last visit: 10/27/2024 Posts: 672 Rating: (147) |
Dear Lucky123 , you need to verify something: In your list you havethe RT library for F-Systems, but I could not find any F-ailsafe I/O module in your configuration. So, either you do not need this software package or you will have to use other I/O modules. Regards. |
Give us your feedback and show us your respect! |
|
This contribution was helpful to1 thankful Users |
4/24/2012 1:56 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
Hi, Just need to know which part number is Rt Library? I am not able to see it, if you can please clarify it bit more.
|
4/24/2012 2:02 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Me also not Understand the What He want to say, I have also not find in the List you have given. |
Ammy |
|
4/24/2012 2:19 PM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
I got the error While Importing the CFG File So i can't able to see your HW. Lucky: Reexported and uploaded the configuration, see attached. 1. You are using only one 6ES7-341-1CH02-0AE0 CP341 Communication Processor, RS-485 then why you want both Master & Slave Software With Dongle, yes, you are correct, I need to have only one master dongle. 2. Selecte the 6ES7 972-0BA60-0XA0 Instead of 6ES7-972-0BA52-0XA0 , a 35 Deg Outlet. Its as per client, so cant change. 3. Also you can go with 32 Channel INPUT & OUTPUT Module for cost effective. Its as per client so cant change
Attachmentsimatic h station(1).zip (446 Downloads) |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
4/25/2012 7:45 AM | |||||
Joined: 12/1/2009 Last visit: 10/27/2024 Posts: 672 Rating: (147) |
Dear Lucky123,
|
||||
Give us your feedback and show us your respect! |
|||||
This contribution was helpful to1 thankful Users |
4/25/2012 8:19 AM | |||||
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
Thank you for your response. Yes, I understand that I posted the list. Your support is appreciated. I will ask client for the clarification on this. However, I would appreciate, if you can please check the configuration and see, if there are any more errors. Since I do not have the actual hardware, I am not sure, if I missed out something. |
||||
Last edited by: Lucky123 at: 4/25/2012 8:21 AM |
|||||
4/25/2012 8:57 AM | |||||
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Lucky, Your Configuration is look Ok, you have consider all the Module Correct, & in my last post I have told you the What you have to consider or Change need. |
||||
Ammy |
|||||
This contribution was helpful to1 thankful Users |
Follow us on