12/3/2007 8:24 AM | |
Posts: 2 Rating: (0) |
How can I safeguard the content of a db in my Pc?. I has the points of an axe in a db and I can modify with an OP270. But if i want to take with software step 7 the real Value doesn't safe. Is possible do that?. I have used the sfc84 for copy ram to mmc but doesn't work . The file in pdf is how i have program the sfc84. Thank! AttachmentESCRIBIR_MMC_OB1.pdf (239 Downloads) |
12/3/2007 2:20 PM | |
Posts: 2 Rating: (0) |
OK! That's work!. But I have used the SFC83 for re-read the values. But in SIMATIC STEP 7 If i look offline the Db has only the init value (0), Thank you!!!! |
Follow us on