2/28/2018 3:27 PM | |
Posts: 64 Rating: (4) |
Hello! I use next module (just 1st channel, other are disabled) - F-DQ 4x24VDC/2A PM HF (6ES7 136-6DB00-0CA0) V1.0 and can't start this module. Attachmentimages.zip (522 Downloads) |
Last edited by: Jen_Moderator at: 3/1/2018 9:25:44 AMAdded all files as an attachment. |
|
2/28/2018 3:39 PM | |
Posts: 64 Rating: (4) |
Parameters by the defaults (I just inserted module to the project from the library). The compilation is completed without errors and warnings |
3/1/2018 6:10 AM | |
Posts: 64 Rating: (4) |
Can anybody explain why I can receive data from other modules in the rack but can't get data from this one? |
3/5/2018 3:52 PM | |
Posts: 64 Rating: (4) |
So, my result is: after I pressed "identification" I've got "module is unreachable"...... (same time other modules are work properly in this ET station) |
Follow us on