7/13/2013 9:09 AM | |
Posts: 1064 Rating: (72) |
post your hardware and we will see if we can help you out |
7/13/2013 10:13 AM | |
Posts: 30 Rating: (0) |
Hi all, 1. Master S7 314C-2 DP 2. 3 ET 200B 32di 3. Power Supply SITOP 24V 20 A serve as power source to the 3 ET 200B and to S7 314C-2 DP Thanks and Regards |
7/13/2013 11:17 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Dear j3pd, Do you remember this thread: |
Ayman Elotaify |
|
7/13/2013 11:53 AM | |
Posts: 30 Rating: (0) |
I try it to Step 7 and also in Tia V11, but seems still i cannot progress. |
Follow us on