4/28/2010 5:57 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
Hi, Follow there is a sample program that emulate a PWM generator in a normal user program timing (i.e. without the help of the special digital output of the CPU). AttachmentPWM.zip (4709 Downloads) |
Last edited by: Pegaia at: 10/19/2010 11:45 AMchange subject only Last edited by: Pegaia at: 4/29/2010 12:16 PMsubject correction Denilson Pegaia |
|
This contribution was helpful to
18 thankful Users |
4/4/2016 2:56 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by DKLEIGH is split to a separate thread with the subject How to power a RC servo motor using the PWM on the PLC?. Best regards |
1/20/2017 1:08 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by ss7479 is split to a separate thread with the subject PWM, generate train of pulses having frequency of 50Hz,100Hz, 200Hz, 500Hz, 1Khz. Best regards |
Follow us on