5/6/2011 9:48 PM | |
Joined: 9/23/2005 Last visit: 8/13/2024 Posts: 4347 Rating:
|
Hi, I attached here a very simple sample program with S7-1200 and Sinamics G120 in Profinet.The ZIP file has the STEP7 V11 Project and the GSDML data. In principle, the main steps are: create a project with a S7-1200 CPU, import the GSDML, drag&drop it to the Network View, drag&drop the connection to the PLC, drag&drop the Telegram 1 to the drive,build a simple logic onOB1, compile all and download all and configure the device name on the drive. Attachmentpn.zip (9167 Downloads) |
Last edited by: Pegaia at: 5/9/2011 10:58 PMLast edited by: Pegaia at: 5/9/2011 12:32 PMcorreciton S7-200->1200 Denilson Pegaia |
|
This contribution was helpful to
17 thankful Users |
5/7/2011 5:39 AM | |
Posts: 15 Rating:
|
Hi! It's interesting! Have you tested the program on real hardware? |
5/9/2011 8:32 PM | |
Posts: 15 Rating:
|
Another error in theme name... |
5/9/2011 10:58 PM | |
Joined: 9/23/2005 Last visit: 8/13/2024 Posts: 4347 Rating:
|
Sorry |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
1/22/2012 11:48 AM | |
Posts: 17 Rating:
|
Dear, I have go through ur prog. and also try with my S7-1200 CPU 1214C and CU240S PN, but it not communicating. i have attachment config. so give me some hint.. manual.. thank u... Regards BNCOE
Attachments71200_cu.zip (2069 Downloads) |
1/31/2012 12:32 PM | |
Posts: 8 Rating:
|
Hi I have tried your sample program in my project but I am not having any luck. I am using a s7 1200 to read the parameters of a G120 CU 240s PN F. It keeps coming up with an error message saying hardware submodule component moved or missing HW ID = 14. I have enclosed screen shots of the program for your viewing. I seem to have established communication ok but this error keeps coming up any time I try to download it to the device. Is it necessary to alter something in the drive to allow the plc to read its' parameters or should it allow access anyway. Regards, Liam Attachments7 1200 screen shots 1.pdf (2670 Downloads) |
2/5/2012 6:48 AM | |
Joined: 8/31/2010 Last visit: 8/8/2024 Posts: 1519 Rating:
|
Hello All, Check this Application Example which is recentlypublished in Applications and Tools --> Connecting a SINAMICS drive to an S7-1200 CPU in TIA Portal (via GSD file) But this application is with PROFIBUS DP |
Last edited by: Ganes10 at: 2/5/2012 9:45 AMmissed to mention abt PROFIBUS DP Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
Follow us on