9/20/2006 9:22 AM | |
Joined: 4/24/2006 Last visit: 7/10/2024 Posts: 8711 Rating:
|
Hello, When you use a CPU314C with MMC the following faq will help you: http://support.automation.siemens.com/WW/view/en/17602317 With the CPU314IFM the option Save Ram to Rom is used to write to the internal Eprom. http://support.automation.siemens.com/WW/view/en/18652056 See chapter 19.1.5.4 If you have a CPU that has the option to use a MMC, You'll have to use it. The CPU will not function without MMC. Best regards, Wizard |
9/20/2006 10:28 AM | |
Joined: 2/22/2006 Last visit: 10/23/2014 Posts: 17 Rating:
|
Hello MadMax, See the following FAQ for details on RAM to ROM and MMC: http://support.automation.siemens.com/WW/view/en/22295462 |
10/23/2006 3:02 PM | |
Posts: 47 Rating:
|
Thanks everyone for the assistance. I now understand the MMC functionality. ABL |
Follow us on