12/11/2019 6:37 AM | |
Joined: 4/18/2014 Last visit: 5/20/2024 Posts: 253 Rating: (5) |
And this is my last query , (for my another project) For Standard Report generation (apart from our customised one) , i can automatically print the report by using HMI tags==>events ==>value change==> print function. (main reason to do automatically is for each day the plant can run more than 20 batches, So after completion of each batch i can move the report in pendrive then it is easy for me to use the same template for all batches) And this document can save in pen drive as pdf document. (please refer the attached) With reference to the the document (Printing with simatic HMI control panels) at Page.No 24 we can set constant file name in string value, but i need to give the individual name for each file w.r.t batch Number. 1.So is it possible to assign the tag for string value in PDF settings.If yes then how? 2.If not than what is the possible way to save each file w.r.t to Batch Production number? (or) If there is any other method to save the standard Report with customised file name as String value (for each batch the batch production number should be a file name) in pendrive (it may be pdf/csv anything). Thanks in advance. ------------------------------------------------------------------------------------------ Attachment58205602_printer_options_package_doku_v12_en.pdf (282 Downloads) |
Last edited by: GUWS at: 12/11/2019 06:41:15Last edited by: GUWS at: 12/11/2019 06:45:47Last edited by: Jen_Moderator at: 12/11/2019 08:36:51New subject after splitting |
|
12/11/2019 6:42 AM | |
Joined: 4/18/2014 Last visit: 5/20/2024 Posts: 253 Rating: (5) |
Standard part of my Batch report is attached and this is an sample one.
Attachment1.pdf (299 Downloads) |
12/11/2019 9:42 AM | |
Joined: 7/5/2013 Last visit: 5/28/2024 Posts: 3091 Rating: (505) |
Hello GUWS, you may find it in this post: posts/wincc-pdf-report-name Regards, Frink |
Pi is exactly three! |
|
12/11/2019 9:47 AM | |
Joined: 3/5/2017 Last visit: 5/28/2024 Posts: 771 Rating: (126) |
There is Wince VBScript command manual there. https://support.industry.siemens.com/cs/attachments/13408815/VBScript_WinCE.pdf There are all commands that you need in that document. There are documents about file handling. https://support.industry.siemens.com/cs/ww/en/view/59885894 https://support.industry.siemens.com/cs/ww/en/view/59604194 |
- Trying is the first step towards failure. |
|
Follow us on