5/30/2015 12:19 AM | |
Joined: 2/18/2015 Last visit: 1/16/2024 Posts: 66 Rating: (5) |
Hello everyone, I'm working on a migration from S5 95U to S7 314c-2DP. I found a SB2 block, but when I opened it like a PB in the STEP 5 software I realized that it was empty. I'm not sure if I can delete it, moreover the SB2 is not called in the program. I attach a picture of the SB2. ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/1/2015 1:10:44 PMNew subject after splitting |
|
Follow us on