5/26/2016 3:08 AM | |
Joined: 9/27/2006 Last visit: 12/4/2023 Posts: 12187 Rating:
|
Hola Jaarroyl; Bienvenido al foro de Siemens. Esta seccion del foro ha escogido Ingles como idioma internacional, para permitir a un numero mayor de miembros de poder intercambiar. Hay otra seccion que usa aleman, siendo que Siemens viene de Alemania. Haznos el favour de usar Ingles cuando visitas el foro; veras que las respuestas vendran en Ingles tambien. Gracias. Hello Jaarroyl; Welcome to the Siemens forum. This section of the forum has chosen English as an international language, to allow a maximal number of members to interchgange. There is another section that uses German, as Siemens comes from Germany. Please do us the favour of using English when you visit the forum. You will find that answers will come to you in English also. Thank you, Now, to answer your question: the following FAQ applies to WinCC v13 Advanced or Professional . With WinCC (TIA Portal) V13, how do you transfer a configuration without a direct data connection to a PC with WinCC Runtime Advanced/Professional? https://support.industry.siemens.com/cs/ww/en/view/103198851 Both the PC where you create the project and the one you want to transfer it to must have the same licenses installed. Note that like many documents from Siemens Support, it is available in Spanish also (see the Language selector at the top of the FAQ). Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/26/2016 3:27:32 AM |
|
This contribution was helpful to
1 thankful Users |
5/26/2016 3:17 AM | |
Posts: 3 Rating:
|
Thanks for the help! Im new on this forum. But I have post the topic in English too. |
Follow us on