1/3/2017 7:07 PM | |
Joined: 9/30/2013 Last visit: 9/23/2024 Posts: 7 Rating: (1) |
Dear Experts. There is a problem with local/remote LogIn to web interface of M874-3 router. The default admin/admin is changed to admin/$NewPassword and device is configured and working good inc VPN connections. After some time after LogOut its impossible to LogIn to the web interface because "Invalid username/password" and only after electrical reset (power off/power on) the Login is possible again. Its not problem of specifical device becouse i have 5 of these devices and same problem is exist in all of them. Thank you in advance ------------------------------------------------------------------------------------------ Closed cause duplicate. Second thread: Scalance M874-3 LogIn issue |
Last edited by: CS Moderator at: 1/5/2017 9:32:27 AMNew subject after splitting Last edited by: CS Moderator at: 1/5/2017 9:34:43 AMlink to second thread added |
|
Follow us on