5/19/2017 12:09 PM | |
Joined: 4/29/2016 Last visit: 4/10/2025 Posts: 31 Rating:
|
hello all, I used SCALANCE X101-1 for communicating 2 Remote I/Os on Fiber Optics . i faced one problem for using it stable. After powering up Scalance and insertion of FO cable, i can monitoring of data transfer between both RIOs and it is working properly, But when power off it ,due to any of reason, it is not become healthy automatically after powering on. For doing system healthy , I have to remove FO cable and further insert into FO port of Module. and that have to repeat for 2-3 time and system become healthy. i am using it for first time, and so i don't know any configuration process of it. Need Help ,THANKS IN ADVANCED ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/22/2017 11:35:04 AMNew subject after splitting |
|
11/15/2017 1:13 PM | |
Posts: 1 Rating:
|
I am facing the same issue. In my case, I have two stations connected between two SCALANCE X101-1 by FO cable. When I restart one of them, the communication is completely lost and not coming back again. If I remove the FO and put it back again, system become healthy. Does anyone know why is this happening? Your help is really appreciated, Thanks! |
Follow us on