10/30/2021 1:22 PM | |
Joined: 7/6/2020 Last visit: 8/3/2024 Posts: 2 Rating: (0) |
Hello fellow Siemens addicts, Got exactly same problem with all XC208 on site. Every day on 22:23:38 connection with PLC drops for 2 seconds, device creates fault like shown in attachment. The problem is that there are no packet losses, no connection drops, fault is just created but nothing else happens - all profisafe devices keep up with connection, all drives and other devices doesn't stop working. In PLC there are faults created looking like that: 39 of 3200; Event ID: 16# 02:39CB Error: IO device failure - PLC Outgoing event Event type: OK 10/30/2021 6:26:25.414 AM (Coding: 16# 34 00 00 05 16 B2 B1 24 97 E4 9D DD 39 CB 00 00 38 CB 00 00 00 00 02 C0 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 40 of 3200; Event ID: 16# 02:39CB Error: IO device failure - XC208 Outgoing event Event type: OK 10/30/2021 6:26:25.350 AM (Coding: 16# 34 00 00 05 16 B2 B1 24 94 15 98 0A 39 CB 00 00 38 CB 00 00 00 00 01 F3 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 41 of 3200; Event ID: 16# 02:39CB Error: IO device failure - Connection abort by IO device XC208 Incoming event Event type: Error 10/30/2021 6:26:23.697 AM (Coding: 16# 34 01 00 05 16 B2 B1 24 31 98 BD 9D 39 CB 00 00 04 BE 00 0B 00 00 01 F3 00 02 00 00 00 00 00 00 00 00 00 00 81 81 FD 0B CF 81 FD 05 00 00 00 00 00 00 00 00) 42 of 3200; Event ID: 16# 02:39CB Error: IO device failure - Connection abort by IO device PLC Incoming event Event type: Error 10/30/2021 6:26:23.630 AM (Coding: 16# 34 01 00 05 16 B2 B1 24 2D 93 BF 18 39 CB 00 00 04 BE 00 0B 00 00 02 C0 00 02 00 00 00 00 00 00 00 00 00 00 81 81 FD 0B CF 81 FD 05 00 00 00 00 00 00 00 00) ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 11/01/2021 14:28:52New subject after splitting |
|
Follow us on