9/23/2015 1:28 PM | |
Joined: 2/9/2015 Last visit: 6/6/2024 Posts: 65 Rating: (1) |
hi dear all please give me example for tia portal v13 this zip file is for v11 i think thank you |
9/23/2015 1:45 PM | |
Posts: 5225 Rating: (1193) |
[1] Try this for some details on scaling.. [2] TIA can handle lower version projects. You open the earlier version project just like you can open other projects (within the TIA software) Go to the "open project" and browse to the project you need to open - go into the folder and get the APxx extension. - xx represent the version number. If the extension is ZAPxx - then the file is an archive project. THAT is opened through the "retrieve" option under "projects" button inside the TIA software. Again higher versions can open/extract lower versions. There is one snag... If you have a lower order license (BASIC), you cannot open a project that has a PLC / HMI that needs a higher order license. For example Step7 Basic will not open an S7-1500 project. Okay? Helpful? |
12/10/2015 5:03 PM | |
Posts: 25 Rating: (6) |
Pejman, If you need to scale your A_IN just implement this formula: Alternatively you can use the blocks from S7-1200 library: https://support.industry.siemens.com/cs/#document/39334504/in-step-7-(tia-portal)-v11-how-can-you-scale-integer-values-in-real-numbers-and-real-values-in-integer-numbers-for-analog-measurements?dti=0&lc=en-WW Pav
|
Last edited by: Pav_ at: 12/10/2015 5:04:59 PM |
|
6/6/2016 7:54 AM | |
Joined: 12/6/2013 Last visit: 2/26/2024 Posts: 66 Rating: (0) |
What happend if I give a value greater or out of the range of min-max on norm_x? |
4/22/2017 6:38 AM | |
Posts: 2 Rating: (0) |
Excuse me! Don't I want to use LIMIT instruction and OUT_Range? |
Follow us on