2/26/2016 7:32 AM | |
Posts: 5225 Rating:
|
The above note is the best place to start from
I have taken the document from post 2/24/2016 5:20 PM and used a mark-up tool to add commentary and placed in into my old post of 2/25/2016 10:24 PM. I do this reluctantly as I know we (you) are moving in the wrong path. ... I agreed with From your supplied link.. (also works up to 27Vdc?) ...this requires for each direction of movement
|
Last edited by: William_B at: 2/26/2016 7:34:18 AMfill up some blanks |
|
2/26/2016 1:41 PM | |
Posts: 5225 Rating:
|
Article to read.. (academical: speed curves) http://www.precisionmicrodrives.com/application-notes-technical-guides/application-bulletins/ab-022-pwm-frequency-for-linear-motion-control |
This contribution was helpful to
1 thankful Users |
2/26/2016 2:35 PM | |
Posts: 5225 Rating:
|
{Set :: Mentor tone} We program because of the hardware and to compliment it. Case in point... PWM vs PTO when using the H-bridge. Step0 - understand what is asked by the project and what the aims are. Step1 - get to know the hardware and what is required. It does not need to be experimentally proven but it must be 99.5% sure from research at least. - - - in the actual hardware you are using. Step2 - configure the hardware on the PLC. Step3 - create a model (design) of rule based or mathematical formula to give control. Step4 - coding Step5 - test, evaluate, adapt. w PWM links to look at.. |
Last edited by: William_B at: 2/26/2016 8:23:51 PMadd coding related links |
|
Follow us on