Industry Online Support
Technical Forum
7/8/2023 11:19 AM | |
Joined: 7/8/2023 Last visit: 7/8/2023 Posts: 1 Rating: (0) |
I recently purchased an XFOC+ Gram scale with an RS-232 connection, and I am having trouble connecting it to my PC. I have a cable that goes from RJ12 to USB, which seems to be suitable for the connection. However, when I attempt to connect the device to my PC, it appears that the scale is not sending any data. My goal is to connect the scale using a Python code, but even though the code appears to be functioning correctly, I am not receiving any data from the scale. I have also attempted to connect using other software such as Putty or Hercules, and while the connection is established, no data is being transmitted. Moreover, I have found that the manual lacks sufficient information. It suggests performing certain operations that the scale does not seem to support. I am in need of assistance to determine whether the scale is indeed sending data or not. Can you explain how I should set the scale for continuously sending data? I would greatly appreciate any guidance and support in resolving this issue and understanding the functionality of the scale's data transmission. AttachmentMANUAL_ZFOC_ES_EN_FR_PT_001.pdf (415 Downloads) |
Follow us on