8/31/2020 2:31 PM | |
Joined: 12/18/2014 Last visit: 11/2/2024 Posts: 34125 Rating: (4249)
|
Import of a technical question via PM form the User Robijn. Hi ixo65, I saw a topic that you replied on concerning displaying an analog value on a KTP400. You gave an example with an analog input of 0-10V, but i still cound't figure it out unfortunately. Now I am working on a project as a beginner and I have connected two analog inputs to an AM2 module (4-20mA) with a range of -1 - 10 bar. I was wondering how I can convert the inputs so that I can read -1 to 10 bar on my hmi of both of them indipendently. In addition, the values must be compared, whereby he must give a message with a difference of 1 bar (can this pressure difference also be read out on an hmi or only the independent inputs?). The rest of the program is working fine, but i'm really stuck here. Like to hear from you!! Kind regards, Robin |
8/31/2020 2:32 PM | |
Joined: 12/18/2014 Last visit: 11/2/2024 Posts: 34125 Rating: (4249)
|
Hello Robijn, you have not written which TIA version you are using. Not even which LOGO! you have and which LSC version. I gave you an example in TIA V13 SP2 with a LOGO! 0BA8.Standard (LSC V8.0) created. I don't think your pressure sensors have a range from -1 to 10 bar. I think 0-10 bar is more likely. Can you write the manufacturer and type of your pressure sensors?
AttachmentRobijn.zip (417 Downloads) |
8/31/2020 3:09 PM | |
Joined: 11/15/2019 Last visit: 10/31/2024 Posts: 63 Rating: (0) |
I use Tia Portal V15.1 and a Logo 8, 12/24 RCE. The pressure sensors are from IFM, type PM1704. On the first page of the attachment you can see the ranges. AttachmentPM1704-00_EN-US.pdf (391 Downloads) |
8/31/2020 3:28 PM | |
Joined: 12/18/2014 Last visit: 11/2/2024 Posts: 34125 Rating: (4249)
|
I have upgrade the TIA project to V15.1. By LOGO! there are two types of 0BA8. Without the order number and the firmware version I can't say if you have a 0BA8.Standard or a LOGO!8.FS4. AttachmentCompare_two_pressures_V13_SP2_V15.1.zip (392 Downloads) |
9/1/2020 8:31 AM | |
Joined: 11/15/2019 Last visit: 10/31/2024 Posts: 63 Rating: (0) |
Thanks a lot ixo65!! I think I finally understand how to do it thanks to your help. Attached is my Logo program with the analogue part at the bottom. The only thing I haven't figured out yet are the correct tag addresses for Pressure_1, Pressure_1-pressure_2 and Pressure_2 in my case. Like to hear from you. Kind regards, Robin AttachmentVeolia.zip (374 Downloads) |
9/1/2020 10:30 AM | |
Joined: 12/18/2014 Last visit: 11/2/2024 Posts: 34125 Rating: (4249)
|
Take a look at my program for Parameter-VM-Mapping. Tools > Parameter-VM-Mapping |
9/1/2020 10:51 AM | |
Joined: 11/15/2019 Last visit: 10/31/2024 Posts: 63 Rating: (0) |
Thank you, everything is workin fine now. Really appreciate it! |
This contribution was helpful to1 thankful Users |
Follow us on