6/8/2014 12:12 PM | |
Posts: 5225 Rating: (1190) |
Another note.. Some PLCs allow time interrupts. These can be set to regular intervals. w |
6/8/2014 1:20 PM | |
Joined: 3/24/2009 Last visit: 7/9/2024 Posts: 535 Rating: (112) |
Dear Sajit, you can find some more information about the interrupts mentioned by William B. here. Hope this helps! Best regards, yy1 |
Last edited by: yy1 at: 6/8/2014 1:21 PM |
|
This contribution was helpful to1 thankful Users |
6/8/2014 5:40 PM | |
Posts: 5225 Rating: (1190) |
Thank you for that link. That would sure help Sajit if he is using an S7-300 / S7-400. Those functions are also available on the S7-1200 (FW4) and S7-1500. @Sajit: Please tell us which PLC and what software are you using? w |
This contribution was helpful to1 thankful Users |
6/11/2014 5:54 PM | |
Joined: 11/3/2013 Last visit: 12/14/2021 Posts: 18 Rating: (0) |
i'm using S7 400 with Step 7 5.5. First i am planning to store the data in sql database and then apply a relatime filter for the first 15 entries as per schedule time earliest. regards Sajit.
|
6/11/2014 5:59 PM | |
Posts: 5225 Rating: (1190) |
Thank you for your reply. Did any of postings help you resolve your question? If not.. please let us know what the issue is. w |
6/13/2014 12:50 PM | |
Joined: 11/3/2013 Last visit: 12/14/2021 Posts: 18 Rating: (0) |
Dear William, my issue is still not resolved. The trigger is not the issue. My machine will create a trigger which I will use to save the time and date of when the activity was done. Then I need to add a particular no of hours to this savedtime and date to get the new date and time for again doing this activity. The same activity is repeated every half hour at different locations (72). thanks |
Follow us on