1/31/2012 11:36 AM | |
Joined: 2/16/2011 Last visit: 3/23/2023 Posts: 229 Rating:
|
Hello; Some samples of basic bit commands in SCL language. See project in Attachment... Regards
AttachmentSCL.zip (1319 Downloads) |
Gabriel de Oliveira |
|
This contribution was helpful to
5 thankful Users |
1/31/2012 3:08 PM | |
Joined: 7/7/2010 Last visit: 3/24/2023 Posts: 13205 Rating:
|
Thanks Gabriel de Ol...,
I looked at the FCs. What if I have a LOT of P_TRIG needs. Do I make them FBs so they can be multi-instance? Same for the RS FF? A single trigger is good. However, withthe built-in commands, they can appear all over the place and work just fine. For an FC, their usefulness is fairly limited. |
science guy |
|
8/4/2015 4:44 PM | |
Joined: 8/4/2015 Last visit: 3/22/2023 Posts: 1 Rating:
|
mr.oliveira please can you send simple worked examples about s7-scl.I tried zip file.it didn't work. thanks |
9/9/2015 9:09 AM | |
Posts: 6 Rating:
|
awesome |
Follow us on