4/9/2020 4:41 PM | |
Posts: 6 Rating: (0) |
Hello Everyone, I Hope you all are having a great Time. The problem I'm facing right now is that I've created a source code in SCL that generates the FB 610. When compiling it any error pops up and everything seems to be fine i'm even able to call it anywhere in my program without any problem but it just doesn't work when downloding it to the PLC-SIM. it looks like it is not executed and the PLC scanner just ignore it. If you guys have ever had something like that before I would appreciate you to let me know how you worked it out Please find attached my project file FB610 is called in FB600 as a multi instance block AttachmentStarting.zip (960 Downloads) |
4/10/2020 1:36 AM | |
Posts: 6 Rating: (0) |
Omg, Thanks man that was embarrassing haha. |
Follow us on