Industry Online Support
Technical Forum
3/27/2009 5:35 AM | |
Posts: 16 Rating: (0) |
Dear All, Ideveloped a program with scout V4.1.0, and deviceFW version V4.1. Now I have installed Sount V4.1 SP1 HF6 . When open the project which wasdeveloped in V4.1 it is not opening. the error disply attached here. ( But When open the project which was developed in V4.0 it is openning whith out any error.) Kindly give me the solution for this. AttachmentScout_v4.1.16.pdf (248 Downloads) |
3/27/2009 6:23 AM | |
Posts: 16 Rating: (0) |
Thak u for ur kind responce. |
Follow us on