3/28/2017 5:56 PM | |
Joined: 10/19/2016 Last visit: 3/25/2023 Posts: 248 Rating:
|
Hello, We have a problem with a Phase engine associated with our drive 6SL3121-1TE31-3AA3. They tell us that they do not know tweak on our 840d, so I ask vs fine-tuning operation. Overview: The spindle rotates at 6000rpm: . In .png instead are illustrated the vibrations to which it is subjected by the 3000 to 6000 rpm spindle body (the last part as seen is critical). at low speed (~1500 rpm) i hear a lot of scratches in the steady speed (they disappear instantaneously if i cut pulses). i know somethinf about p1460 and p1715 for loop control but less more. The bearings do not heat despite the vibrations, so i do not yet know whether the problem lies in the resulting configuration to the MIS or to a mechanical. |
Last edited by: gtsolid at: 3/28/2017 5:57:19 PMEngineer, runner, 棋手 |
|
Follow us on