1/4/2018 3:39 PM | |
Posts: 4 Rating: (0) |
hello, I work in a factory where the integrator has installed a PC with a resolution of 1366 x 768, the display is full screen, there is no problem. I want to change the program but when I send the program on the PC the display is too small, I have several resolution options but not 1366 x 768. do you know which version of wincc I have to install to find this resolution? thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/6/2018 11:24:27 AMNew subject after splitting |
|
1/6/2018 11:55 AM | |
Posts: 8946 Rating: (999) |
WinCCflex2008 SP3 or higher. |
This contribution was helpful to2 thankful Users |
1/8/2018 1:35 PM | |
Posts: 4 Rating: (0) |
Sorry, i don't written but i use the sp3 |
This contribution was helpful to1 thankful Users |
1/8/2018 4:15 PM | |
Posts: 4 Rating: (0) |
Thank you very much for your help, i have installed Update 7 for WinCC flexible 2008 Service Pack 3 : https://support.industry.siemens.com/cs/ww/en/view/19241467 And now i have the good resolution |
Last edited by: Jen_Moderator at: 1/17/2018 2:10:17 PMInserted right link. |
|
This contribution was helpful to2 thankful Users |
Follow us on