4/14/2023 7:31 PM | |
Joined: 1/21/2013 Last visit: 9/18/2024 Posts: 3114 Rating: (486) |
Hi tecnoproject, To be honest, I can't follow your description. Can you please share some images that illustrate your problem? Please provide some additional information. Which version of WinCC Unified are you using? What image version do you have installed on your MTP1200? Have you tried using the latest V18 image version? This can be done even if a previous version is used for engineering. Kind regards |
4/19/2023 8:00 AM | |
Joined: 1/21/2013 Last visit: 9/18/2024 Posts: 3114 Rating: (486) |
Hi tecnoproject, Your screen windows will be displayed with the z-order you build in the project. There is no way to change the order of screen elements within this layer, nor to move them to another layer. You should try using OpenScreenInPopup instead. Kind regards |
4/19/2023 10:19 AM | |
Joined: 1/21/2013 Last visit: 9/18/2024 Posts: 3114 Rating: (486) |
Hi tecnoproject,
No, you can have multiple pop-ups open on your screen at the same time. You will need scripting if you want to limit it to a single pop-up. See the FAQ "How do you control pop-up windows in WinCC Unified PC RT and Comfort Panels via script (JavaScript examples)?".
In general, PC Runtime and the panel should show the same behavior. To ensure that this is corrected, you should create a support request to report this to Siemens. Kind regards |
Follow us on