8/29/2022 7:43 AM | |
Joined: 8/3/2009 Last visit: 9/16/2024 Posts: 13694 Rating: (1726)
|
Hi basically you can simulate scripts of a Panel project also in the Simulation on PC. But some objects are not accessable as in Windows CE like on the panel. for example access to file system. here the Objecs and syntax is different: Panel: LINK PC: LINK Here is some other FAQ which shows differences. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on