12/26/2009 7:03 AM | |
Joined: 12/23/2009 Last visit: 6/9/2024 Posts: 9 Rating: (0) |
I have a block valve FESTO, with code like this:
1. VIGA 03-FB-4 (18,656 L307) - 4 Digital Output 2. VIGA 03-FB-4 (18,656 L307) - 4 Digital Output 3. VIGE 03-FB-8 (18,655 L307) - 8 Digital Input 4. FB9-03 (18739 L307) - Profibus station 5. VIGM-03-4, 0 (18,652 L302) - 2 valve 6. VIGM-03-4, 0 (18,652 L302) - 2 valve 7. VIGM-03-4, 0 (18,652 L302) - 2 valve 8. VIGM-03-4, 0 (18,652 L302) - 2 valve 9. VIGM-03-4, 0 (18,652 L302) - 2 valve 10. VIGM-03-4, 0 (18,652 L302) - 2 valve 11. VIGM-03-4, 0 (18,652 L302) - 2 valve 12. VIGM-03-4, 0 (18,652 L302) - 2 valve The sorted order from left to right. I configured the Profibus network to block FESTO valve but no corresponding GSD file, you do have this GSD file, please help me! Thank you very much!! Note: I tried using GSD files downloaded from multiple sites wep network (attachment). In the file, I tried to configure the network are many ways, but they are not suitable! I set thinking, this is too old GSD file, it can not find where to configure the network! Sorry for my English!! AttachmentFB9-03_GSD.zip (250 Downloads) |
This contribution was helpful to1 thankful Users |
12/26/2009 10:23 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, Did you look here? Profibus (GSD) 11/2009 Generic Station Description files (GSD) and bitmaps for Festo valve terminals http://www3.festo.com/__C1256D56002E7B89.nsf/IndexCat?OpenFrameSet&Location=E&Company=INT&Language=EN&Query=FIELD+shPK1+CONTAINS+FeldbusGSD/EDS+AND+FIELD+Company+CONTAINS+INT+AND+FIELD+SpracheGesamt+CONTAINS+English |
Best regards |
|
12/27/2009 9:35 AM | |
Joined: 12/23/2009 Last visit: 6/9/2024 Posts: 9 Rating: (0) |
I have downloaded the GSD file on wep and tried to configure the block valve, however, the modules in the "FESTO Type 03 FB9" only type 1 byte or more. Therefore can not configure network. The work I do is upgrade the control system of Siemens: S5 to S7. Profibus network configuration of the S5, see attachment. Configured S7 replaced respectively: 1. Simatic S7-300, stabilized PS307 Power Supply, 120/230V AC, 24 V DC 6ES7307-1EA00-0AB0 2. SIMATIC S7, CPU 315-2DP: 6ES7315-2AG10-0AB0 3. DI16xDC24V, Interrupt: 6ES7 321-7BH00-0AB0 The ET200M and ET200L not changed. See project file Please help me!! , thank you!! AttachmentProject S5-S7.zip (153 Downloads) |
12/27/2009 5:03 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, In annex the GSD files found on the Festo support pages. There is a read-me file with pictures. Should explain what GSD must be used depending on the model. If I look to your component list, Ihave the feeling that the GSD in the folder FB9-03 should be OK. The correct GSD is the one having the correct Ident_Number(corresponding to the ident number built in thedevice itself). I guess that you expect to find 2 bit modules in the GSD, but when working with standard GSDs for Profibus,the smallest unit for standard Profibus is a byte. And you have to add the inputs and outputs together to get a global amount of inputs and outputs. And configure the slave in S7 with an I have added in the annex a manual found on the Festo support pages. In that manual, at chapter 4.2,they explainthe working with Siemens, for the IM308 (S5) and S7 (Step7 V4)as well. I hope this help. Attachmentfesto.zip (323 Downloads) |
Best regards |
|
This contribution was helpful to1 thankful Users |
6/25/2014 1:53 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoS5 to S7 conversion - how to traced the input and output adressand closed. With best regards, Narrator1
|
Follow us on