8/10/2016 6:51 PM | |
Posts: 116 Rating: (2) |
Hello, How to use secomea to remote access the Simatic PLC and HMI? |
8/10/2016 7:05 PM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello Automation Program; This is how Secomea proposes to connect to a remote Siemens PLC: http://secomea.com/siemens-remote-access/ One example: TIA Portal: TCP connection via native Siemens Ethernet port The following describes how to connect via the Siemens TIA portal to a Siemens S7-1200 PLC equipped with an Ethernet module that is attached to a SiteManager via Ethernet (directly or via an Ethernet switch). Please note; if you are connecting to a Siemens HMI, you need to set the transfer method on the HMI to “Ethernet”. Furthermore, you will not be able to “Go Online”, but you can download to the HMI. See Appendix C – Changing transfer method on Siemens HMI on how to change the transfer method on the HMI. Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
8/10/2016 9:07 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, other link if can help you: http://www.gate-manager.it/app_notes/Siemens_guide_full_v2.1.pdf |
This contribution was helpful to2 thankful Users |
8/11/2017 12:05 PM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
New question published by mihaiTC is split to a separate thread with the subject In TIA portal v13 can go online/ download with the PLC but can't download the program in the HMI.. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on