Industry Online Support
Technical Forum
3/21/2007 12:43 PM | |
Posts: 661 Rating: (123) |
Hi, it is possible. If you don´t want to wire switches you can use - the cursor keys (upper half of the attached program) or - softkey (lower half of the attached program). The explanationfor the user is displayed in the message texts. Is that the answer to your question? AttachmentTest_.zip (1013 Downloads) |
3/22/2007 9:12 AM | |
Joined: 1/25/2006 Last visit: 10/13/2024 Posts: 257 Rating: (60) |
Yes, it is OK. Thank you for help. |
Follow us on