6/15/2012 10:33 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Hello, in this power range the 1PH8 would fit. The motor exists as synchronous and asynchronous version, forced ventilation and water cooling. Please follow the link: https://intranet.automation.siemens.com/mcms/mc/en/motors/motion-control-motors/simotics-m-main-motors/simotics-m-1ph8/Pages/simotics-m-1ph8.aspx Configuration manual: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=de&objid=46484744&caller=nl Unfortunately the latest version 5/2012 is currently only in German available. The EN version 4/2010 includes not the current portfolio. The latest version in EN will be to download in about 4...6 weeks. You could use the tool SIZER to select in easy way a possible motor: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=28311063&lang=en&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&subtype=130000&nav0=index&objid=10804987&idx0=&idxSrc0=sizer CAD-files via www.cad-creator.com HP 250 means 184KW For example 1PH8284-1xC4 with 171KW @ 700rpm. The motor existswith different rated points (windings).Bigger motors available as well. Attached the characterisitc curve of the motor above. Attachment1PH8284-1.C4.pdf (421 Downloads) |
With best regards, |
|
6/17/2012 5:55 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello TechTeam, Thank you very much for your reply. As mentioned in my earlier post, this is heavy duty lathe. Maximum job loading capacity is of 40T. This main DC motor is used to rotate & brake such huge mass. (DC drive is of 4Q)To the best of my knowledge, the starting torque of DC shunt motor is very high & running torque is constant from low speed to its base speed range. With this 1PH8 series motor, is it possible to havesame motor characteristics as that of DC motor i.e. achieve high starting as well as constant, torque during normal rotational speed? Thanks & regards, DEEP. |
Last edited by: PISCEAN 2010 at: 6/17/2012 6:29 AM |
|
6/17/2012 7:03 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, When trying to open above link, getting error meassage. Please find attached here with the screen shot of error message. Is there another way to visit or see above link information? Thanks, DEEP. |
6/19/2012 2:29 PM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Hello, sorry, the link is only for internal use. Please try this one: https://www.automation.siemens.com/mcms/mc/de/motoren/motion-control-motor/hauptmotor-simotics-m/simotics-m-1ph8/Seiten/simotics-m-1ph8.aspx You can see the motor characteristic attached. Constant torque from start up torated torque. Attachment1PH8284-1.C4.pdf (370 Downloads) |
With best regards, |
|
7/4/2012 1:47 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, What you say is true. Kindly note in my case, present DC motor torque is 5936 Nm upto 300 RPM. The 1PH8284-, 184 Kw motor rated torque as per chart is 2333 Nm upto 700 RPM which is 60% less than the required torque. Hence I think this won't be anequivalent motor.Please see the attached sheet. Do you agree this point? Regards, DEEP. Attachment1PH8284-1.C4[1].pdf (407 Downloads) |
Follow us on