3/27/2014 1:09 PM | |
Posts: 3 Rating: (0) |
Hello, I have a problem with FB block for sending UDP packets. It is possible for the SIMATIC S7-1200 to send a UDP packet as a broadcast packet? I used TUSEND, but I not posted nothing. You can do some simple example? Here is my test program. But I do not know why it does not work. Thank you ... AttachmentTEST.zip (707 Downloads) |
Last edited by: CS Moderator at: 4/1/2014 12:25 AMnew subject after splitting from /tf/WW/en/Posts/46768#top |
|
This contribution was helpful to1 thankful Users |
4/1/2014 3:44 PM | |
Posts: 3 Rating: (0) |
Hello... Much as I can understand... When I want to send a UDP or TCP packet, you must use the first function - TCON? And then, for udp - TUSEND and tcp - TESEND? |
4/3/2014 8:03 AM | |
Posts: 3 Rating: (0) |
Hello, This is not true. If you do upgrade Simatic S7-1200 to version 2.x, so it supports. |
4/3/2014 11:56 AM | |
Posts: 1368 Rating: (126) |
i also mean open communication... look at the picture in the attachment. Greetings |
Follow us on