12/21/2017 3:07 PM | |
Posts: 36 Rating:
|
[snip] I would like to create following system: s7-1200 connected to Access Point and Client conneted with second s7-1200 I would like to send data between the drivers. What configuration of network shall i set in Tia Portal? I tried to this using three methods: 1.I tried to configure them in two separate subnets, but i found out that there is problably no way to transfer the data - both drivers were set as IO controllers, and there were two separate subnets so i cannot use get/put instruction - FAIL 2.Then i tried to configureone subnet - created profinet network with 4 nodes: 1 Io controller s7-1200, AP, client and io device s7-1200. But the effect was that S7-1200 returns error for 10 seconds, then work normally for 10 seconds and once again return error - FAIL 3.Finally i tried to configure project without scalance modules, but effect is the same plus AP and client red led is lighted - FAIL Important thing is that I use non Siemens antenna - its antenna of external producer. The only parametr of antenna I passed is an antenna gain. Cable lenght is 0 and i havent inputted additional attenuation parameter. Can anybody tell me in what way shall i configure this network? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/22/2017 7:31:17 AMNew subject after splitting and Division of questions into separate topics. |
|
Follow us on