10/8/2008 11:11 AM | |
Posts: 8 Rating: (0) |
First I would create a program for PC which would send an SMS andreceive a text message as a parameter. Then I would create GMsgFunction() which is called every time when a message appears and which would call the program which sends SMS About GMsgFunction() http://support.automation.siemens.com/WW/view/en/15350783 |
10/9/2008 1:48 PM | |
Posts: 86 Rating: (1) |
Thanks alot Darius |
10/18/2008 12:03 PM | |
Joined: 1/29/2006 Last visit: 5/7/2024 Posts: 446 Rating: (64) |
There was a similar discussion about sending SMS on this forum, few months ago. I have solved this task with use of 3rd party software (see this link: http://www.klinkmann.com/gsm/gsmprice.htm and see a product with code PR000673 or PR00067, "GSM-Control V4.44 SMS Center software for PC"). This SW works as OPC client (WinCC works as OPC server...). You can trigger SMS on changes of states of binary variablesof Wincc,..... . You can format messages,.... . Bit unfortunatly, you can not directly import complete Alarm messaging from SCADA application to GSM-SMS application, because this application supports only OPC-DA access. Some work has to be done, but it is simple and also reliable. Have fun! uel123 |
6/12/2012 4:45 PM | |
Joined: 11/10/2010 Last visit: 4/26/2024 Posts: 165 Rating: (8) |
helo this software is not free? ther's no a free version for evaluation or a demo?
|
6/21/2012 5:26 PM | |
Joined: 9/17/2007 Last visit: 4/17/2023 Posts: 799 Rating: (82) |
Hello, maybe you hove a look on PageControl. There is an "ready to use" solution (for WinCC). You can buy an (tested) package with a mobil modem also... unfortunately i found no english version of the informel website... |
VG / regards vanDyk |
|
3/29/2015 3:13 PM | |
Joined: 10/31/2006 Last visit: 9/21/2022 Posts: 134 Rating: (33) |
Have a look at this and see if it might help. |
7/2/2015 6:31 AM | |
Joined: 5/12/2012 Last visit: 10/26/2023 Posts: 4 Rating: (0) |
Hi All, Alarm Control Center (ACC) is a best tool. But if you want to use another (cheap/simple) application, you can follow these is 3 steps : 1. create exe application. *i create Send_SMS application, you can download it. 2. edit Alarm Logging and check Trigger Action. 3. edit script of GMsgFunction. Please visit here : http://hadiscada.blogspot.com/2015/07/send-sms-for-wincc-alarm.html to download Send_SMS application and more detail about 3 steps above. Regards, Hadi. |
Last edited by: Hadi_MAD at: 7/2/2015 6:33:18 AM |
|
Follow us on