5/3/2017 7:33 AM | |
Posts: 102 Rating: (10) |
im not pro in s7-300 who can help me ... i have a 2 wire pressure sensor [-1 to 60 bar range] and want to read it by 4-20ma current at S7-313C With AI 8x12BIT my pics attachment's is so clear & obvious ... if my wiring is wrong or has a solution im happy to tell me Sir's AttachmentProblem.zip (262 Downloads) |
Last edited by: Wormus at: 5/3/2017 7:35:52 AM |
|
5/3/2017 7:48 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi Wormus, can you measure the current on the wires? What about the measurement-range module on the side of the module? It has to be in D Also try it with both sensor-wires on the card. A 2-wire-transducer is normally supplied by the card. More on the wiring and the settings of the card you can find in the manual, chapter 6.7: SIMATIC S7-300 S7-300 Module data hope this helps, regards, |
FCK WAR! |
|
Follow us on