12/13/2007 5:46 PM | |
Posts: 7 Rating: (1) |
Dear Navnag, True, that to change the default assignment of data block information in basic type we need Switch ES. The basic type 1 ,contains 4 data blocks of phase currents & binary status information. All the requirements of Farzad are fulfilled by default basic type 1 itself. SoI dont think that Switch ES is needed to be used. Please refer the attachment also. AttachmentBasicType1.zip (504 Downloads) |
Last edited by: nawaz_fly at: 13.12.2007 17:47Last edited by: nawaz_fly at: 13.12.2007 17:47 |
|
6/26/2014 3:03 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoSENTRON WL communication (COM16) - MODBUS. With best regards, Narrator1
|
10/9/2014 4:33 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
Follow us on