1/13/2011 11:27 PM | |
Posts: 69 Rating: (3) |
Dear ADSU, We are using same username and password for all the three pc.But it shows" user is not having rights to open".It shows when we open wincc in server & client.we are configured as workgroup only.And then when we download from esos to server at that time it shows sql server doesn't have access rights. RGDS R.R
AttachmentDURING OPENING WINCC IN SERVER&CLIENT STATION.pdf (193 Downloads) |
Last edited by: R&R at: 1/13/2011 11:33 PMLast edited by: R&R at: 1/13/2011 11:30 PM |
|
1/14/2011 11:49 AM | |
Posts: 288 Rating: (22) |
You can have XP on ES and OS Client/Stand alone station For OS Server Windows Server 2003 is mandatory. |
1/19/2011 8:33 AM | |
Posts: 69 Rating: (3) |
Dear Nil96, my configuration in folder is like that.kindly see the attachment and tell me the remedy. RGDS, R.R
AttachmentCONFIGURATION IN CLIENT & SERVER STATION.pdf (200 Downloads) |
Follow us on