6/21/2015 12:51 PM | |
Joined: 1/17/2007 Last visit: 7/2/2024 Posts: 115 Rating: (2) |
Hi all I have a project in which there are two pumping stations. At each station there is an OS Server that is used Wincc V6.2. I've run 'OS project editor' and The 'Split Screen Manager Function' as described in ID: 24193022 used to call my customized Faceplate . Now I want to use OS of station 1 as client of station 2 . How do I add 'server prefix' to Tags of customized object in pictures and its faceplate.Note that the pictures of both stations will be displayed in same process window of station 1. |
Best Regards |
|
6/22/2015 11:58 AM | |
Joined: 1/17/2007 Last visit: 7/2/2024 Posts: 115 Rating: (2) |
Hello Georg Thank you for your attention. As I said before the process pictures of station 1&2 will be displayed in one picturewindow and therefore the objects in the process pictures of station 2 require 'server prefix' while it isn't true for station 1.Similarly ,one picturewindow is showing faceplates of both stations and only station 2 require 'server prefix' ( 'Tagprefix' in ID: 24193022 is derived from properties of objects and therefore I don't know how attached 'server prefix' to 'Tagprefix'). |
Last edited by: bijan at: 6/22/2015 12:09:18 PMBest Regards |
|
Follow us on