3/16/2016 5:05 PM | |
Joined: 7/9/2013 Last visit: 8/30/2019 Posts: 10 Rating: (1) |
Hallo all, we have commissioned a redundant OS system. But after sometime, there seems to be re-occurring Redundant alarms (see attached jpg file). I have already done the following actions but not successfull.
Did any of you face a similar situation? Could you also advice me what to do in this situation? What to check, maybe any reference links, manuals? I have additionally attached the latest diagnostics files (SysLog) files. System configuration:
Any contribution will be highly appreciated. Attachmentdiagnose files.zip (123 Downloads) |
3/17/2016 1:24 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
A few things that came up in my mind: - Is the terminal bus in Simatic Shell selected? - Is the terminal bus on the first place in Simatic Shell? -What are the actual values of the internal tags: @RM_MASTER of both servers? One should be "1" which indicates master -Did you once activated runtime of the OS server on the ES station? Maybe you can take a look at the following Siemens page. It's all about diagnostics. Maybe you can post some diagnose files for us?
|
Last edited by: Oreca at: 3/17/2016 1:29:35 PMIf I could help you, you can use the RATE button. Thank you. |
|
3/17/2016 4:15 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Can you upload the diagnose file: "SIMATIC_S7_Protocol_Suite_01" of both servers and ES? |
If I could help you, you can use the RATE button. Thank you. |
|
3/18/2016 5:42 PM | |
Joined: 7/9/2013 Last visit: 8/30/2019 Posts: 10 Rating: (1) |
Hallo oreca, here are the log files (upto date). Maybe i have missed to note something. Thanks in advance. Regards Santhosh Attachmentdiagnose 2016 03 18.zip (70 Downloads) |
3/21/2016 11:08 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello Santhosh, Server 1 seems to have a network error, which could be related to the network card or connections Did you setup your network card correctly (like sleeping mode set to off). Are there any problems with it. Maybe a connection issue. Are the Simatic Shell settings correctly configured (activated redundancy)? |
Last edited by: Oreca at: 3/21/2016 11:11:21 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on