4/18/2024 4:23 PM | |
Joined: 3/19/2019 Last visit: 10/28/2024 Posts: 104 Rating: (0) |
Hi, In our case also, Servers are frequently going to fault state or lossing the connection. When I trace the issue, we found the timestamp differ issue and CcUaDAS service has stopped and restarted. The timing of timestamp differ issue and CcUaDAS service has stopped and restarted issue and servers went to fault state or losing the connection is same. Is this all the things are co-related? For additional information, our servers also virtual servers and IT deprt taking backups everyday basis. But we are facing this issue since 10-4-24 onwards only.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/19/2024 09:48:25New subject after splitting "If you want the answer - ask the question" |
|
4/19/2024 9:52 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Servers are frequently going to fault state or lossing the connection is published within the conference SIMATIC WinCC. Best regards, |
Follow us on